Part Number: SN74LVC1G04
Other Parts Discussed in Thread: ASH
Hi,
I am doing power calculation for this IC.I gone through the below document

After that I done this calculation.Can you please verify:-
Vcc=3.3V,Icc=10uA Static PD=Vcc*Icc=0.033mW
Cpd=18pf,Fi=10Mhz,Ni=1 Transient PD=Vcc*Vcc*Fi*Cpd*Ni=0.196mW
Cl=15pf,fo=10Mhz(assume),Nsw=1 Capacitive PD=Vcc*Vcc*Fo*Nsw=1.63mW
So total PD(max)= Static PD+Transient PD+Capacitive PD=3.63mW
So I can Consider the maximum power dissipation of SN74LVC1G04 3.63mW.
I think this is too much low value. Is it right calculation for Power dissipation??
Thanks