Other Parts Discussed in Thread: SN74LVC1G17
Team-
Do we have any devices that could replace the LT6994 in a customer design? I don't see much under delay elements, but I might have overlooked something and would like a confirmation.
Thanks,
Alec
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74LVC1G17
Team-
Do we have any devices that could replace the LT6994 in a customer design? I don't see much under delay elements, but I might have overlooked something and would like a confirmation.
Thanks,
Alec
We don't have anything with the same functionality as the LT6994, however we could recommend a simple replacement - a Schmitt-trigger buffer with an RC filter on the input. The RC filter is there to eliminate noise/spikes and will also add a small amount of delay to the rising and falling edges of the output. I would recommend starting with RC values of 4.7kΩ and 100pF. (τ= 0.47μs)
The SN74LVC1G17 comes to mind as an option.