Part Number: TXS0102
Other Parts Discussed in Thread: DM3730
We are using TXS0102 to level shift 1.8V I2C signal coming from master(DM3730) and on some boards we are not seeing the I2C clock on the output of level shifter.
Based on datasheet for TXS0102, inoput sI2C low signal has to be < 150mV. Based on DM3730 datasheet, at higher sink currents master clock low can be as high as 360mV.
Could someone confirm if these two parts are compatible?