Part Number: TXB0108
Hi
I read the datasheet which is mentioned as below,
What happen to output and input if the input current is lower than 2mA?
Also I read the follwing post. However I do not understand why this device need the input current more than 2mA.
( I need some a simple mechanism.)
Our customer asked us that they wonder why you are not specified this current to electrical specification if this is very critical.
We need to talk with our customer about this. So please give some concerns why and what will be happen if the current is lower than 2mA.
Regards,
Koji Hamamoto