This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: SN74LVC1G07 Open-Drain connection/level

Part Number: SN74LVC1G07


We are considering SN74LVC1G07 in our application, if our Vcc is 1.8V, can the open-drain output be pulled up to 3.3V on this device?

  • Hi Ken,

    Yes. This device can have inputs and outputs above Vcc, which allows for up and down translation applications.

    This is indicated in the Absolute Maximum Ratings table under "Vo - Voltage range applied to any output in the high or low state"