Hi,
When VCC is 1.8V, what is spec for VOH and VOL? Thanks!
Regards
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi David,
The values specified by 'Vcc = 1.65V' are for a standard voltage supply of 1.8V +/- 0.15V. 1.65V is the worst case for this, so the values are specified there. You can directly apply the drop on the output to 1.8V.
For example, at VCC=1.65V, IOH = -4mA, TA = -40C to 85C, VOH = VCC - ΔVO = 1.2V, ΔVO = 1.65V - 1.2V = 0.45V
ΔVO will be the worst case at 1.65V, so we can use that value for 1.8V:
At VCC=1.8V, IOH = -4mA, TA = -40C to 85C, VOH = VCC - ΔVO = 1.8V - 0.45V = 1.35V
Hi Emrys
Thanks for feedback! So for VOL, is it similar? For 1.8V and IOL=4mA, ΔVO=1.65-0.45=1.2, then VOH=1.8V-1.2V=0.6V, right?
Regards
David
For VOL, the difference is from ground instead of from VCC, so a 0.45V VOL rating should still be 0.45V at VCC = 1.8V.