Part Number: SN74HC595
Other Parts Discussed in Thread: SN74AHC595, TPIC6C595, SN74LV595A, CD74ACT164, CD74ACT299
Hello,
I'm considering TI's SN74HC595 for my new application, and have some questions when I saw the SN74HC595 datasheet as below.
1. below text means that SNx4HC595 use Low-drive CMOS device, so there would be no ringing problem due to overshoot or undershoot? Am I right?
2.As for the below, the max source(driving) current per port is 35mA and total 70mA at VCC 5V condition.
How about at VCC 3.3V condition?
And does TI recommend using sink current? If there's no problem to use, please let me know the current limitation for sink current.
thanks,
TS