Part Number: CD4059A
Other Parts Discussed in Thread: SN74HC4060, SN74LVC1G80
I have a 16kHz clock. I want to divide it by 2^15 or 32768. The high voltage is 1.8V and low voltage is 0V. Do u have a IC that can do this ???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CD4059A
Other Parts Discussed in Thread: SN74HC4060, SN74LVC1G80
I have a 16kHz clock. I want to divide it by 2^15 or 32768. The high voltage is 1.8V and low voltage is 0V. Do u have a IC that can do this ???
Dear Michael,
Thanks for your reply.
Do the ICs you've mentioned also meet my criteria for high and low voltage, i.e. , if I input a 16kHz clock with a high voltage of 1.8V and a low voltage of 0V, will the ICs output a clock pulse of high voltage of 1.8V and a low voltage of 0V.
Hello,
You are absolutely correct, the device I mentioned previously actually will not work at the 1.8V spec you need.
1.8V is a little bit more difficult to be able to acheive. While these solutions are not optimized, they seem to be the best options we have.
1. Use 4x http://www.ti.com/lit/ds/symlink/cd74ac161.pdf
This will do the frequency division in stages.
2. If you can take the original solution that I provided, but supply the HC4060 device with 2V, then it will actually be able to "understand" an input voltage of 1.8, and output a 2V signal. I understand this is kind of an odd solution, but it is a possibility. You could then power the second stage SN74LVC1G80 with a 1.8V supply and the inputs would be overvoltage tolerant to 5.5V, and would then down translate the output voltage to the 1.8V level that you need.
Best,
Michael