Part Number: SN74GTL2010
Hi
our application is 1.8V(FPGA) to 3.3V SPI flash, as below..
On U6 Pin 17 (SPI_DI),,, It can't pull down to 0V ( about 1.1V) so it can't control SPI flash normally.
Can you tell me how to solve this issue ? thanks a lot
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74GTL2010
Hi
our application is 1.8V(FPGA) to 3.3V SPI flash, as below..
On U6 Pin 17 (SPI_DI),,, It can't pull down to 0V ( about 1.1V) so it can't control SPI flash normally.
Can you tell me how to solve this issue ? thanks a lot
Hi Shreyas,
Do you mean increase pull up register on S or D side to 10k?
My application :
SPI frequency about 20MHz.
the signal driver direction as below. those are my test record
1. all pull up register=4.7K... U6 pin 8 always 1.8V.( U8 can't pull it to 0V)
2. all pull up register=180... U6 pin 8 , U8 can pull it to 1.1V , can't pull to 0V)