This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can I use TXB0108 to level shift SPI, CAN interface, Audio, RGB LCD, Interrupt signals(all 1.8V to 3.3V) and UART(1.8V to 5V) ?
For I2C I plan to use TXS0108E.
If these cannot be used, please suggest the alternate one for each interface.
Regards,
Shanu V
The TXB has weak outputs in order to allow bidirectional signals (the output must allow being overdriven by another device).
As far as I can see, none of your signals are bidirectional, so you can use a direction-controlled translator. How many signal lines do you have? Any frequency requirements?