Part Number: CD74FCT245
Other Parts Discussed in Thread: CY74FCT245T
Hi,
The datasheet of the CD74FCT245 claims to limit the output voltage swing to 3.7V, the electrical characteristics list a minimum value of VOH, but, is it safe to assume that the max value won't go above 3.7V (without pull up resistors)? If pull up resistors were used, is it also safe to assume that the dual-diode voltage drop of the output stages will be overridden?
On the other side, the CY74FCT245T claims a typical VOH value of 3.3V under specific load conditions. What would be the maximum expected VOH with and without pull up resistors?
Regards
JS