This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC244A: Power Supply Recommendations

Part Number: SN74LVC244A

"Each VCC terminal should have a good bypass capacitor to prevent power disturbance.

A 0.1 μF capacitor is recommended for devices with a single supply.

If there are multiple VCC terminals, then 0.01 μF or 0.022 μF capacitors are recommended for each power terminal."

(SN74LVC244A Datasheet(SCAS414AB) / Page 11)

Q. What is "Each VCC terminal" and  what are "multiple VCC terminals"?

    SN74LVC244A has only one VCC so I don't know exactly what meaning is.

    I have four SN74LVC244A devices and connected same voltage source - 3.3V at VCC.

    What is the recommended capacitor value?