Part Number: TX517EVM
Dear TI Employees,
Following the user manual, I have set up our TX517EVM. After power up, I try to show the output 1 and 2 on our oscilloscope (our oscilloscope is capable of receiving 200Vpp signal). However, I cannot see any results. I believe the board is not generating any signal. I've also tried connecting TX517EVM output to TX810EVM input, and then connect TX810EVM output to our oscilloscope . Still I cannot receive any signal.
Here is a photo of our TX517EVM after power up. Please verify if leds are properly on and off. As you can see in the photo, LED 1, 3, and 7 are off. According to the manual, LED3/7 mean FPGA alive.