I'm re-designing a VME-bus system that uses 5V on many cards. I plan to re-design one card at a time to use 3.3V. This means each card must maintain a 5V interface on the bus. The current design uses 74HCT640 for the data bus and 74HCT240 for the address bus. Both of these are inverting devices. I'd like to find similar inverting devices that accept 3.3V from the card logic and 5V from the bus. It appears as though the SN74LVCC3245A would be ideal except it is not inverting. Please suggest a replacement device(s).