Hello,
I am looking for a level shifter that converts 0-3V pulse input to +2V to -2V output swing. This pulse switches at a frequency ~1MHz to 100MHz. But our duty cycle is very small ~2% of 1MHz - 100MHz. We are fine selecting any one frequency between 1MHz-100MHz depending on the availability of the level shifter. Let me know if there are any level shifters available.
Also, let me also know if there are any level shifters close to this specs.

We are planing to go with YZP package. We have following questions: