Part Number: SN74LS04
Other Parts Discussed in Thread: SN74LVC04A, SN74LVC14A, SN74HCT14, SN74HCT04
Hi,
I am using SN74LS04 for an on/off sensor detection, For some reason, my channel 1Y is not able to pull above 0.9V when my input 1A is 0V. If 1A is 5V, then my 1Y will pull low to 0V. I thought there is a leakage somewhere else, but all my other gate are 2A, 3A, 4A are working as expected with a identical circuit. All your inputs are greatly appreciated.
Thanks