This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: High Capacitive Load

Guru 20090 points

Part Number: TXB0108
Other Parts Discussed in Thread: TXS0108E

Hello,

Our customer would like to use this device for 200pF capacitive load.
In the datasheet P.14, the TXB0108 is designed to drive capacitive loads up to 70pF.

Are there any method to drive this high capacitance by TXB0108?
Could you please let me know the device which can be used for this?

Signal Frequency is 20MHz
VCCA=1.8V, VCCB=3.3V

Best Regards,
Ryuji

  • Hi Again,

    I have additional question.
    Could you please let me know the maximum output load of TXS0108E?
    Can this device drive 200pF output load?

    Best Regards,
    Ryuji
  • Hey Ryuji,

    I think you'll be hard pressed to drive a load that large with this part, but fear not, there may be a work around. If you want to provide more drive then you can parallel two or more of the output lines together. If you do this you will need to ensure that the outputs that are tied together are driven by the same input signal on their respective input pins. Obviously the downside to this probably means having two, or more, translator IC.

    Another option for you could be to add a series resistor on the output to increase the impedance. Although this would help with driving more capacitance, you're going to be hit with a performance decrease. This resistance will give you a RC circuit and will begin to limit the datarate. For you, this solution is not advised since you want to go 20MHz.

    I'm glad you brought up the TXS series of devices. I was going to recommend you take a look at these since they can handle higher capacitive loads at the expense of minor speed hits. This ability to handle the higher capacitive loads working in tandem with two+ channels tied together I think is your best bet for driving your desired load.

    Best Regards,
    Nick

    If this answered your question, please hit the green "Verify Answer" button! If not, let us know and we'll answer any remaining questions that you have.
  • Hi Nick san,

    Thank you for your support.
    I will suggest that parallel using to high capacitive load drive.

    Also could you please let me know the extent of how much capacitive load the TXS 0108E can drive for 20MHz data rate?
    Could you please share the load capacitance vs. data rate information ?

    Best Regards,
    Ryuji

  • I'm not sure of an exact figure to point you toward the characterized value. Let me see if I can dig something up for you.

    Nick
  • Hi Nick san,

    Thank you for your checking.
    I'm looking forward further information.

    Ryuji
  • Hi Nick san,

    Our customer connected the two inputs/outputs and evaluated.
    As a result, it got worse than before it was connected.
    I think that there is a problem with some configuration.
    I would like to obtain a circuit diagram from the customer and confirm it.
    For customer confidential, since I want to send mail directly instead of E2E, can you contact me at the address below?

    asaka-r@clv.macnica.co.jp

    Best Regards,
    Ryuji
  • Hey Ryuji,

    I've PMed you, send me the documentation that you have in when you get a chance. I'll also order some sample of the part you're using and see if I can replicate a similar type of issue or maybe get successful operation!

    Nick