Other Parts Discussed in Thread: TXS0102, LSF0102
Hi ,
I am using PCA9306 for transfer 1.8V I2C and ether MDIO/MDC signals to 3.3V.
Please suggest me if there is any other part which is same or better in performance.
Thanks & Regards,
Madhu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Madhu,
Do you need buffering or do you only need translation/level shifting? Also, what mode will you operate at? Standard, Fast Mode, Fast Mode Plus???
I have attached a selection guide link below.
http://www.ti.com/lit/an/slva787/slva787.pdf
-Francis Houde
Hi Francis,
The value 2.5MHz is not of any I2C device, but an ethernet PHY's MDIO interface ( Marvell's 88E1111).
I am planning to use same level translator device for both MDIO and I2C interfaces.
Whether TCA9517B can be used for both of these interfaces?
Regards,
Madhu
Hello Madhu,
Unfortunately we don't have anything that supports these high data rates in I2C group. Your best bet is either the LSF0102 or the TXS0102 translators. I know they both support open drain. I just don't know max data rates at what cap load. I am moving this to the Translation E2E. They should be able to help you better.
-Francis Houde