Part Number: TX517EVM
Other Parts Discussed in Thread: AFE5809EVM, , TX810, TX517
Hi,
We have made a fully functional sonar system using the following EVMs:
TX517EVM -> Transducer -> TX810EVM -> AFE5809EVM -> TSW1400EVM
Here is a photo of our result:
The two large amplitudes shown are generated by our pulse generator (TX517EVM). Our TX517EVM uses the default configuration, except we have change two things. Pattern depth is 5 (Table 5 of slou317c manual) and PRF is 1 (kHz). As you can see, the pulse is generated for a very short time (only about 40 samples).
My questions:
Why the generated pulse is very short? It's just about 40 samples, in terms of time it's 0.6 milliseconds! Is it fine that the pulse is so short? We're using this EVM for sonar application.
The OUTA of our TX517EVM is directly connected to Input of TX810. Correct me if I'm wrong, but I don't need OUTB of TX517EVM, right?