This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108-Q1: Package Dimentions

Part Number: LSF0108-Q1

How do I find the appropriate width x height dimensions in mm for this parts package (PW)?

  • Hey Sarah,

    You can simply look at the overall dimensions in the link that you provided. The package dimensions will be the largest overall dimensions that don't reference the pins. In addition to knowing this you should also realize that dimensions will have a tolerance associated with them and that can be seen by the fact that there are two numbers on top of each other. Take the average of those two figures to get the ideal dimension.

    As an example, the part you have in question would be 4.4mm x 6.5mm for package dimensions.

    If this answered your question, please hit the green verification of answer button below! If not, then feel free to ask more questions, I'll stop by the thread again.

    Best Regards, 

    Nick