Other Parts Discussed in Thread: CD4504B
Hi, I need to convert 15V logic to 5V logic for my application. I saw two ICs CD4050B and CD4504B that seemingly can do this, looking at the datasheets. Is it correct that both can do the logic level conversion from 15V to 5V? If yes, is there any preference between the two? I see that there are different propagation delays, but I don't really need anything too fast anyway, so the delays in both the chips look acceptable.