Other Parts Discussed in Thread: SN74LVC3G14,
Hello,
I want use SN74LVC3G14 as a Level shifter. (Vcc=5V)
- When I stet the Input to a 5V Level everything is Ok (Icc = 55uA)
- But when I set the Inputs to 3,3V-Level the IC needs about 11mA per Channel, why?
Test:
(3-Ports = 0V, 0-Ports = 3,3V -> ~0,055mA)
(2-Ports = 0V, 1-Port = 3,3V -> ~11mA)
(1-Ports = 0V, 2-Ports = 3,3V -> ~22mA)
(0-Ports = 0V, 3-Ports = 3,3V -> ~33mA)
- (extra) current flow into Vcc, not into the Inputs
- there is no output resistor, current I(out)=0mA
- The pinning on PCB is OK, because with 5V Inputs everything works correct!
- I also tested it with „74HC3G14“ (Nexperia) on the same PCB this one works perfekt!
- I also tested it with SN74LVC3G04 and it’s also the same problem as with SN74LVC3G14!
- I testet it on different PCBs and it’s the same problem!
Other Test
- Vcc = 3,3V = Input-Level=3,3V -> Icc = ~0,055mA undependet on any Input-Level, works perfekt
- Vcc = 4,5V > Input-Level=3,3V -> Icc = ~1mA per Input_Channel High!
Markin Code ist "14CZ" (SN74LVC3G14DCUR VSSOP)