Im having a strange issue with TXS0108EPWR
I do have a following sonncetion of the mentioned part:
The strange thing is, that on pins A4 and A6 Im having the proper 3v3 -> 5v output, but on the A5 the inout (checked) is the same as for A4 and A6, but the output on the B side is 0.3V for high and goes below 0V for low with - see the following image (taking about the last line)
First line of image is proper B output on A4, second line is the input for A5 and third line is the output for B5
The connection is absolutely the same. I have also replaced the TXS0108E and the result is the same.
Any ideas? Leads? How to debug this situation?
Thanks,
Marcel