Part Number: TXB0106
Hi,
I am using voltage level translator Part # TXB0106.
I have a query on the VOL and VOH levels.
I am giving supply to the port as per below configuration:
VCCB = 3.3V, VCCA =1.8V
Note that my device is operating in the 0°C to 50°C environment.
Based on the above table VOLA max @ temperature –40°C to 85°C is 0.4V max, But my device can accept 0.35V max as an input.Is it create any problem ?? what is the value of VOLmax @ 0°C to 50°C ??
Same for the VOH min @ –40°C to 85°C is VCCA-0.4 = 1.4V min, But my device can accept 1.5V min as an input.Is it work or create any problem ?? what is the value of VOLmax @ 0°C to 50°C ??