Part Number: CD74HC4046A
Other Parts Discussed in Thread: CD4046B, SN74AUC08, SN74S08
Dear team,
My customer would like to have clarification on this part, could you please assist ?
"We use the reference CD74HC4046APWR to replace the reference CD4046BH (mounted in a hybrid case being replaced). In introduction to the CD74HC4046 datasheet it is written: “The HC4046A and HCT4046A are high-speed silicon-gate CMOS devices that are compatible with the CD4046B”.
Then why the PC3OUT output of the CD74HC4046APWR circuit is called ZENER on the CD4046B circuit?
In fact this does not embarrassed us because we do not use output PC3OUT output. However when we use a reference instead of another the operations are not identical. For example, for the same values of R1 / R2 & C1, the output frequency of the VCO is not the same. Is there a look up table to match the output frequencies of the 2 references ?
Generally speaking what are the compatibilities and incompatibilities between these two components ?"
Thanks, Maxime