What is the short circuit current rating for the SN74LVC2240A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Matthew,
The SN74LVC2244A isn't characterized for short circuit current. The recommended maximum output current is 12mA, although the device is likely capable of driving 50+ mA at a shorted output. Note that the absolute maximum rating of the device is 50mA per channel and 100mA total across all channels - so exceeding either of those values could damage the device.
Hi Emrys
Thanks for your reply. I came across a TI document called "Designing with Logic" SDYA009C. Table 2 in the document specifies the short circuit current (Ios) for several logic families. The SN74LVC240 was specified as 55mA. I would expect the SN74LVC2244A to be lower since it has 26 ohm equivalent resistors on its outputs. I have looked at several datasheets , for example the SN74LVC240, and have not seen the Ios numbers published. It seems that document SDYA009C is the only place the Ios numbers are published.
The output impedance of these devices (LVC family) typically are around 25 to 35 ohms. Assuming the worst case, the output would be ~50 ohms at 3.6V ~= 72mA @short circuit.
As far as I know, there are only two reasons to add a series resistance to a signal line. One is to limit current, and the other is to improve signal integrity. The added resistor is really there to help with signal integrity -- ie to reduce ringing at the distant end.