Part Number: SN74ALVC245
There is one description as belows in the datasheet Page 2:
absolute maximum ratings over operating free-air temperature range (unless otherwise noted)†
Continus current through VCC or GND +/-100mA max
If my customer need driver 8 channels simultaneous with 15mA output current per channel.
That is 15*8=120mA > 100mA
What will happen to the SN74ALVC245? Will it burn down?
If so, can you tell me which device will be suitable for this case?
Best regards!