Part Number: TXS0206
Other Parts Discussed in Thread: OMAPL138, ,
hi dear supporting team,
customer is using flying wire to connect from their brd to our TXS0206 EVK, connect with OMAPL138. and meet below issue:
1. if VCCA goes up ealier than VCCB, there will be ringing happens as below plot, when powering up, OMAPL138 is also in reset status.
2. if VCCB goes up earlier than VCCA, then everything is normal.
3. in nromal operation, if reset OMAPL138, there will be same issue happens.
the sch is as below, they did not include the serial 24Ohm resistors in it. EN is connected to VCCA. if powering up TXS0206 and then provide EN, then everything is ok.
so double check with you:
1. if EN direct connect to VCCA, is there any power up sequence requirement?
2. what's the root cause of such issue? is it due to the bug of the chip? anyway to avoid?