Part Number: LSF0102
Other Parts Discussed in Thread: LSF0204,
Hi,
We have an MDIO hot swap application that also requires level translation. Would like to use either the LSF0102 or LSF0204 parts. In our application, the backplane interface is 3.3v, this is the hot swap interface. Internally, the other side is either 2.5v or 1.8v.
For either LSF parts, will they handle the hot swap situation, done on the 3.3v side? Datasheet for LSF0102 mentions this in a bullet, but it does not discuss. The I/O pins would see voltage initially, at 3.3v, however both vref pins and the EN would be unpowered. After powerup, the VrefB side would be powered on, with EN pulled high also. VrefA would remain unpowered until firmware decides to turn that interface on. This could be quite a while.
Are there any issues when either vrefA or vrefB is unpowered, but the other side is powered, for either LSF0102 or LSF0204 parts?
Is there any incorrect behavior if the LSF0102 EN pins are not powered, but the VrefB power is applied? They are always shown connected, but we may wish to have another control point. LSF0204 seems to separate this entirely. Would that be a better choice if this is necessary?