Other Parts Discussed in Thread: LSF0108, SN74AVC2T45, SN74AVC1T45
Hello,
I need a bit of help so I can choose appropriate voltage level converter for my application.
I need to translate between 1.8V (WiFi LSR Sterling LWB5) and 3.3V (iMX6 SoC) on SDIO interface.
The SDIO on iMX6 can work at up to 200MHz.
I am considering two options for voltage level translators:
TXB0108 vs LSF0108
Which one is more suited for the job?
Thank you!