This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

74LVC1G123



 

Tolerance of 74LVC1G123DCTR

 

If I tune the RC values for 74LVC1G123DCTR one-shot to get a pulse of 400ns, I want to know the variance of the time if I install 10,000 pieces of 74LVC1G123DCTR chips on the same board. The acceptable value is between 380ns and 420ns. Does anyone know the timing error range for this one-shot?

 

Sam

  • Designing with the SN74LVC‍1G123 Monostable Multivibrator (SLVA720) says that the pulse length depends on the temperature and supply voltage, but the largest variations come from the tolerances of your R/C.

    It appears there are no numbers for the accuracy of the internal 0.63212 × VCC voltage threshold.

  • Hi Sam,
    In my tests, I have seen less than 1% variance from our device over temperature - when I exclude the resistor and capacitor from the test chamber. Unfortunately, I do not have test data across all possible process/voltage/temperature variations, so I cannot guarantee this for all situations.

    We typically tell people to only use these devices in situations where they need an approximate delay - for example when you want to reset a processor for "a few microseconds" an MMV is a good solution, or when a delay needs to be "at least" some value.

    In theory, if you can get great capacitors/resistors for the external timing circuit, then this part could maintain the timing you want. I would probably recommend going with a more precise technique for your application.