Hi Team,
In SN74AVCBH16245 datasheet page1, "Active bus-hold circuitry is provided to hold unused or floating data inputs at a valid logic level. Use of pullup or pulldown resistors with the bus-hold circuitry is not recommended.".
1. Does "Control Signal" also support BUS HOLD feature?
2. Unused input pin floating is recommended for bus hold buffer case?
3. If customer place pull-up resistor to input/output signal for initial setting when buffer or driver output siable case. I think recommended pull-up resistor value exisitng for use bus hold and that related with IBHLO and IBHHO spec, would you let me know recommended pull-up resistor value for input/output?
Thank you.
Best Regards,
Jade
Active bus-hold circuitry is provided to hold unused or floating data inputs at a valid logic level. Use of pullup
or pulldown resistors with the bus-hold circuitry is not recommended.Active bus-hold circuitry is provided to hold unused or floating data inputs at a valid logic level. Use of pullup
or pulldown resistors with the bus-hold circuitry is not recommended.