This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: Possible to tied /OE with V_CCB instead of V_CCA?

Part Number: TXB0104


Hi,

In the datasheet, it mentioned that /OE (Output Enable Control) should be tied to V_CCA.

Can /OE tied to V_CCB_3.3V where V_CCA_1.8V is always present?

The reason of doing this is to disable the device (TXB0104 where no output on port B) when V_CCB_0V (pull to ground through load switch output). When load switch is enabled, V_CCB = 3.3V and the device is enabled.

 

Or should we use the partial power down condition mentioned below?

Thanks.

Best regards,

Gim Song

  • Hi,

    The partial power down condition is being deleted in my previous post.

    Below is the partial power down conditions from app notes (scea043.pdf):

    Under partial power down conditions, the outputs are also disabled and put into a high-Impedance state.
    This feature is referred to as VCC isolation. If VCCB = 0 V, the A-port is disabled. Likewise, if VCCA = 0V, the
    B-port will be disabled. In addition, the TXB type translators are fully specified for partial-power-down
    applications using the IOFF feature. This IOFF circuitry disables the outputs, preventing damaging current
    backflow through the device when these devices are powered-down.

    Thanks.
  • Gim song,

    The OE is overvoltage tolerant and hence can be tied to Vccb without issues as long as both are within the recommended operating conditions of the datasheet.