My customer is looking to use the SN74AVCH8T245 with a display controller. The display controller has a VIL of 0.2xVDD, at 3.3V this is 0.66V. The SN74AVCH8T245, has a specified max VOL of 0.7V @ 3V and Io = 12mA. Would this number be lower if less current was used?
Thanks,
Daniel