This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ALVCH16245: Active Bus-Hold output state in HiZ mode

Part Number: SN74ALVCH16245


I am working on an application that needs to disable outputs when a Hi-z state is entered.  I chose this part because we care about having a minimum propagation delay for timing purposes, but this part has bus-hold circuitry.  From my understanding, and this previous thread, The value of the output is held when changing from enabled to Hi-Z.  If this is controlling gates, then the gate would be held on, which is not what we want to occur.  

The datasheet says it recommends not to use pull-up/down resistors, however, we are not using this part to control a bus. It is being used in a uni-directional fashion that may need to be disabled (all outputs Low) in a specific circumstance. Would it be acceptable in this use-case to use pull-downs on the output side? and If not, are there any similar products that are in production for 3.3V logic with similar propagation delay and no bus-hold circuitry?

  • Hi John,
    Unfortunately, the bus hold circuitry really doesn't get along well with pull-up/down resistors.

    I would recommend switching to the SN74LVC16245. The tpd at 3.3V is 1 to 4ns - only 1 ns different from the ALVCH device's 1 to 3ns.