Part Number: TXB0108
I have a question about a TI level translator PN: TXB0108RGYR I want to use in my design
I am working in an application where it is important to keep all A and B outputs of the part in Hi-Z until VCCA and VCCB are up and stable
I have an active low signal that will remain low until both voltages are stable and it is connected to the OE pin. Also have a pulldown resistor on OE pin.
The Data sheet indicates that VCCA <= VCCB during normal operation after power up.
During Power up the order of turn on for VCCA and VCCB is not critical(so VCCA<VCCB if VCCB=0V) since there is a sensing circuit that keeps all outputs in HiZ as long as the OE pin is held low.
I cut and paste section 10 of the data sheet that appears to support these assumptions:
10 Power Supply Recommendations
During operation, ensure that VCCA ≤ VCCB at all times. During power-up sequencing, VCCA ≥ VCCB does not
damage the device, so any power supply can be ramped up first. The TXB0108 has circuitry that disables all
output ports when either VCC is switched off (VCCA/B = 0 V).
The output-enable (OE) input circuit is designed so that it is supplied by VCCA and when the (OE) input is low, all
outputs are placed in the high-impedance state. To ensure the high-impedance state of the outputs during
power-up or power-down, the OE input pin must be tied to GND through a pulldown resistor and must not be
enabled until VCCA and VCCB are fully ramped and stable. The minimum value of the pulldown resistor to ground
is determined by the current-sourcing capability of the driver.
Question???
1. Will the A-B I/O remain in HIZ through states 1-5???
2. According to the datasheet, the outputs are supposed to be in tristate as long as VCCA or VCCB are at ground or OE = logic 0.
Assuming that OE is pulled high, At what voltage level for VCCA, VCCB during turn on do the outputs leave tristate?
State 1: VCCA = 0V VCCB = 0V OE =LOGIC 0 A-B OUTPUTS = HIZ
State 2: VCCA = 0V VCCB = RAMP OE =LOGIC 0 A-B OUTPUTS = HIZ
State 3: VCCA = 0V VCCB = 3,3V OE =LOGIC 0 A-B OUTPUTS = HIZ
State 4: VCCA =RAMP VCCB = 3.3V OE =LOGIC 0 A-B OUTPUTS = HIZ
State 5: VCCA = 1.8V VCCB = 3.3V OE =LOGIC 0 A-B OUTPUTS = HIZ
State 6: VCCA = 1.8V VCCB= 3.3V OE =LOGIC 1 A-B OUTPUTS = LOGIC LEVEL