This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1T45: 1.8V level transaltor

Part Number: SN74LVC1T45
Other Parts Discussed in Thread: LSF0101, SN74AVC1T45

I have a customer who is having a hard time making a serial data bus work at 50MHz (100Mbps).  The problem looks to be the SDO from the IC back into the FPGA.  So they are looking for a non-inverting buffer / level translator that can run at >100Mbps at 1.8V logic.  They are, of course, board area limited so looking for the smallest package (assuming good inventory).

 

They are currently using the SN74LVC1T45 (DSBGA package) for other circuits on the board, but in the datasheet it states that the max data rate at 1.8V is 75Mbps.  Any suggestions?

 

FYI... my first thought was the LXF101 but they want a direction pin - and specifically requested no "auto-directional stuff ."

 

Please let me know.  Thanks, John Garrett, TI-AFA