This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: Can TXB0104 be connected to another TXB0104?

Part Number: TXB0104


We're developing a module to interface to a 3rd party module that uses TXB0104 level shifters on its DIO outputs.  Our module requires level shifters as well.  Can we also use the TXB0104?  This would result in two TXB0104s being connected together.  Will the part work correctly when connected to another TXB0104?  The complete interconnect would be as follows:  2.5V FPGA I/O <-> TXB0104 2.5V to 3.3V <-> TXB0104 3.3V to 2.5V <-> 2.5V FPGA I/O.