This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: SN74LVC8T245

Guru 13485 points
Part Number: SN74LVC8T245


I’m looking for information I could not find in TI’s datasheet.

We have SN74LVC8T245  In our design and I could not find “rise time” in datasheet or Fmax (on the website it says “F @ Nom Voltage (Max) (Mhz) =100” but this is not in the datasheet)

Can you advise if  this device can  works at 100MHz ? can you please check the Rise/fall time?

  • Hi eli,

    This device can be operated at 100 MHz, however signal integrity will depend on loading and supply voltage. I don't have test data for 100 MHz, so I can't guarantee anything about signal integrity at that speed, however, I can say that the device will have better quality output signals at 5V operation than at 1.8V simply due to the output resistance.

    There is no specified output rise/fall time for this device - or any logic device. This depends on the loading in your circuit and the output impedance of the device at the operating voltage.

    You can estimate the output edge rate from the output resistance and load capacitance (Rout = VO/IO):

    tro ~= 3*Rout*Cload