Part Number: SN74LVC2G07
Hi,
With SN74LVC2G07 output connected as below, how to calculate if the pull-up resistor value is ok or not? Thanks!
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC2G07
Hi,
With SN74LVC2G07 output connected as below, how to calculate if the pull-up resistor value is ok or not? Thanks!
Antony
These are not pull-up resistors but current-limiting resistors.
They look as if you wanted to get 20 mA. But the LED forward voltage has large tolerances, and you did not take the buffer's output impedance (max. 25 Ω at VCC = 3.3 V, 11 Ω typical) into account. And the LED intensity has large tolerances, too, so there is no reason to aim for exactly 20 mA.
64.9 Ω is from the E48 series, which is more precision than you'd bother to use. Just use 56 Ω or 68 Ω.