This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual bus buffer from 3.3V to 5V with single supply

Other Parts Discussed in Thread: SN74LVC2G125

Hi,

The customer is looking for the dual bus buffer from 3.3V to 5V with single supply. For example at SN74LVC2G125, to output 5V, the Vcc need to be 5V then the minimum VIH will be 3.5V (0.7V x 5V). This can't be used for 3.3V input. So please let me know if you have the bus buffer for this purpose. Actually the customer want to replace TC7WT125FU from Toshiba.

Best Regards,
Satoshi / Japan Disty