This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: May SN74LVC8T245 Port B input maximum input current should be 50uA (ΔICCB)?

Part Number: SN74LVC8T245


Hi Sir 

May SN74LVC8T245 Port B input maximum input current should be 50uA (ΔICCB)?

May we check why spec have no minimum value? It means don’t care about minimum?

                                    Bogey

 

  • Hi Bogey,

    There is a great explanation of these specification in the application report "Understanding and Interpreting Standard-Logic Datasheets" (page 45-46)

    Yes, the ΔICCB spec should be 50 μA. Note that the test condition indicates that the input is being held at VCCA - 0.6V, which will increase the shoot-through current of the input. This is actually a very good value -- many CMOS inputs have a rating of 500 μA for ΔICC.

    We do not provide a minimum value for this, on any device. We do not recommend designing a system based on a minimum spec (which would likely be under 1uA), as this could result in system failures and is a very bad practice.