Other Parts Discussed in Thread: SN74HC08
Hi team,
Could you please check what are the VIH & VIL levels for SN74HC08 with VCC = +5V? The datasheet only specified VCC =3, 4.5 and 6V.
Many thanks.
Best Regards,
Wei-Hao Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please check what are the VIH & VIL levels for SN74HC08 with VCC = +5V? The datasheet only specified VCC =3, 4.5 and 6V.
Many thanks.
Best Regards,
Wei-Hao Chen
Hello Wei-Hao,
I want to mention first that VIH and VIL are not threshold values. You might already know this, but I see many of our customers get confused by this, and I want to make sure it is mentioned first. These are input noise margin limits.
Note that the given datasheet values are exactly 0.3 VCC (for the VIL spec) and 0.7 VCC (for the VIH spec). At 5 V, these values are:
VIH = 3.5 V
VIL = 1.5 V