This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC00-Q1: High temperature operation

Part Number: SN74HC00-Q1


Hi,

 I am looking at gates that can work up to 140 degrees C operating for an automotive application.

Is there any device that can guarantee it? Or do we have any selection?

Our datasheets specify 125 degrees C max for all versions I looked at.

Internal power dissipation is close to 0, because the device works at 100 Hz.

Thanks

Umberto