This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Successive Approximation Register

Anonymous
Anonymous


Does TI have a Successive Approximation Register IC or logic diagram?

  • Hi Handy Andy,

    We have quite a few SAR ADCs available, and while the basic operation for them is the same there are slight differences depending on the number of inputs, interface type, etc. I'd be happy to help you select a device if that is your goal, but I would need more info on what you are looking for (number of inputs, resolution, speed, interface type, etc.)

    For more general information on SAR ADC operation and designing with a SAR, I recommend checking out our Precision Lab video series covering ADCs.

  • Anonymous
    0 Anonymous in reply to Evan Sawyer

    I am not looking for a complete ADC but was just looking for the register part alone because I am doing a logic exercise for a course I am taking and it requires the logic part alone.

  • All of our devices will be a complete system: sample/hold circuitry, comparator, register, DAC, and possibly other parts depending on device. You may be able to find a way to use discrete components to build a discrete register, but we don't have a standalone register.

    As far as the devices we have, I'd recommend considering the TLC0820A. Parallel at such a low resolution is unusual these days, so we don't have many options there.

  • Hi Andy!
    You can use a ring counter to enable in series x number for number of bits of D type transparent latches with their D inputs connected together with their outputs connected to a DAC; for the IC you could either build one with "discrete" logic devices or use a TI PAL or microcontroller.
  • Anonymous
    0 Anonymous in reply to Evan Sawyer
    Thanks for the help, I will look into the TLC0820.