Part Number: SN74LVC1G34
Other Parts Discussed in Thread: SN74AUP1G34
I am looking at the SN74LVC1G34, which has Ioff. The datasheet says the maximum leakage current into an output is 10 microamps when Vcc is at zero volts. But I would like to find something an order of magnitude (or two) lower than that. I need a 1-gate part, and everything will be at 3.3V when powered up. Is there a logic family that has very low leakage current?
Edit: It looks like SN74AUP is what I'm looking for. Does that sound right?