Part Number: TXS0108E
Other Parts Discussed in Thread: SN74LVC8T245, SN74HC244, SN74AHC244, TXB0108, LSF0108
Hi Team,
I try to drive optocoupler directly from device output B.
The optocoupler connected to 5V and 270 Ohm resistor to the TXS0108EPWR output.
When I try to drive '0' to the TXS0108EPWR output the output low level is ~2.5V instead of ~0.5V as expected.
The current I expected to sink into the TXS0108EPWR output is -12mA.
Please advise.
Thanks in advance,
Shai.