This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC125A: Power Supply Sequencing and the Output Pins

Part Number: SN74LVC125A

Are the output pins safe to be pulled up to a voltage other than VCC that is below 5V?  In particular, I am concerned about having a pull-up on the output signal since I was going to use it as an open-drain device (grounding the input pin and using the output enable pin to control the output).  Will the pull-up resistor back drive into the SN74LVC125A's Vcc when the buffer is not yet powered?

On a related note, I would expect that in this configuration I should only get an output of GND or high impedance, but I think that I am seeing the output being actively driven high as the buffer's power supply is coming up, but it may be from a different source.

  • Hi Josh,
    This device's absolute maximum rating for the output voltage is Vcc + 0.5V, so having the pull-up supply on with the buffer supply off will violate the abs max (and likely back-power the rail).

    In order to be sure that the ouputs start in high-impedance, they OE pin should be connected to Vcc through a pull-up during power on (until it can be driven by the system controller).