Part Number: TXB0104-Q1
Other Parts Discussed in Thread: TXS0102-Q1, LSF0204
Hi Team,
We would like to use TXB0104-Q1 for I2C.
I understand that TXS0102-Q1 is reccomended for I2C, but VIH and VIL of TXS0102-Q1 doesn't meet our spec.
Since we need bi-directional level shifter for I2C, 4ch products are best.
Since LSF 0108-Q1 is 8-channel product, I think that TXB 0104-Q1 is best if it can be used for I2C in a bidirectional level shifter.
I would like to judge whether TXB0104-Q1 can be used for our purpose.
It is written that any external pull up or pull down resister are recommended larger than 50k ohms in datasheet.
I think that this constraint is due to the drivability and will affect VOH and VHL.
If pull-up resister is 30k ohms, VOH and VOL will meet our spec.
If VOH, VOL satisfies the requirements in our system, can it be used with a pull-up resistor of less than 50kΩ?
Please let me know if there are other restrictions and check points.
Best regards,
Tomoaki Yoshida