Other Parts Discussed in Thread: SN74HC541, SN74AVC16T245, SN74LVC16T245
Hi team
Looking at the datasheet P.1, there is a description "Support Mixed-Mode Signal Operation on All Ports (5-V Input/Output Voltage With 3.3-V VCC)".
Does this mean following things are acceptable?
case 1. Input voltage = 5V, output voltage = 3.3V at Vcc = 3.3V
case 2. Input voltage = 3.3V, output voltage = 5V at Vcc = 5V
I guess the case 1 is no problem. How about the case 2?
If the case 2 is not good, are there any devices that can satisfy both cases?
Regards,
Noriyuki Takahashi